Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPWF04S Firmware 1.1.0

Posted on September 28, 2017 at 04:06Hello,I was planning to use the SPWF04S module in a product where all the processing is done in the stm32F439 embedded in the module. It seems like the only way to load an application code is to go through the uP...

STM32F407xx with BlueNRG-1 connecting problem

Posted on April 23, 2018 at 11:20Hello everyone! I'm currently working with STM32F407xx application and trying to connect it to BlueNRG-1 via SPI.All that I have are RESETN and SPI MISO, MOSI, CLK and CS pins connected to bluetooth module. I'm tried...

Lenoe by Associate II
  • 1408 Views
  • 1 replies
  • 0 kudos

Resolved! Why I receive unreliable SCAN_RSP data?

Posted on May 10, 2018 at 14:35Hi,My device is Bluetooth LE peripheral that is based on BlueNRG-2 and STM32 connected via SPI.I would like to present some measurement data in SCAN_RSP to central devices.The measurement is performed every 1 second an...

Resolved! SPWF01 recommended for new designs?

Posted on June 08, 2017 at 18:19Hi Jerry,is the SPWF01 recommended for new designs? Do you have planned any firmware updates for future?Since the SPWF01 will not support IPv6, but the SPWF04 do, I don't see any reason to use the SPWF01 in the future...

SPWF01SA

Posted on May 02, 2018 at 21:40What is the status of  SPWF01SA modules?This link:http://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.htmlsays it is NRND,while this link:http://www.st.com/en/wireless-connectivity/spwf01s...

ax0018 by Associate III
  • 987 Views
  • 1 replies
  • 0 kudos

Is the ST-PLC app source code available?

Posted on May 03, 2018 at 21:21I am evaluating the STM32ODE PLC.  The choice of Ladder Logic items is rather limited.  To add additional items requires modifications to the Android app.  Is the Android project downloadable for modification?#plc #st_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.