Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Packet counter in blueNRG

Posted on June 22, 2018 at 09:54Hi everyone,I would like to count packets which I send in advertising channel. How can I do it? Maybe could I send each packet manually with any function? Then I will be able to increase my counter after sending one p...

Mary W by Associate
  • 1009 Views
  • 1 replies
  • 0 kudos

IDW01M1 (SPWF01SA) Hands-on training issues

Posted on July 14, 2018 at 08:12Hello everyone! I'm new here and this is my firt question.I've been trying for a while to use the X-NUCLEO-IDW01M1, with poor success: I can't even build the example projects in the X-CUBE-WIFI1 software expansion pac...

ST-LINK CLI ''run application to exit''

Posted on July 16, 2018 at 13:51Hello guys!I'm trying to build an automation that involves flashing and reseting an STM32F407 MCU.I'm using ST-LINK CLI V3.2.0.0 in order to do so.My problem is, that when I try to reset the MCU using -Rst -Run the ST...

Getting HTTP POST to work on SPWF04S

Posted on July 12, 2018 at 19:49Hello, I am trying to get a simple HTTP POST command to work. I am using http://ptsv2.com to host a server. I tested the server using curl command in ubuntu, so I know the issue is not there. What I am doing for HTTP ...

IRDA RECEPTION ERRORS AT 38400bps

Posted on July 06, 2018 at 07:27Hi,I'm using a Nucleo-F401RE whith HSE at  9.8304MHz.I try to receive, on UART6, IRDA frames of unknown dimension : from 4 to 60 bytes max; the third code received specify, by a table, the length of the frame. (STX, D...

PB for L152RE: UART1

Posted on July 12, 2018 at 16:59Hello,I have a pb with UART1 for L152RE board. I connected a sensor to my board in UART2 through a Max232 and i succeed to have information to my hyperterminal (TerraTerm). But i was not able to have information in th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.