Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using BLE 5.0 Data Length Extension on BlueTile

Hi,I'm working on the new BlueTile board  (STEVAL-BCN002V1B) including a BlueNRG-2 module. According to documentation, BlueNRG-2 should support data length extension from Bluetooth 5.0. Has this feature already been added to the SDK ?It seems that th...

LStru by Associate
  • 810 Views
  • 0 replies
  • 2 kudos

Using the BlueNRG with FreeRTOS

I try to use the BlueNRG in conjunction with the FreeRTOS but the system always ends up in a hardfault as soon as I querry the BLE services.The initialization of the BlueNRG works and establishing a connection works as well. But it seems like any use...

aj.sk by Associate III
  • 2741 Views
  • 4 replies
  • 1 kudos

Can i build a L2CAP channel using "LE Credit Based Connection request" signalling command in X-NUCLEO-IDB05A1?

Hello Experts,I am looking to establish a L2CAP "CONNECTION-ORIENTED CHANNELS IN LE CREDITBASED FLOW CONTROL MODE" using "LE Credit Based Connection request" signalling command.I am using two X-NUCLEO-IDB05A1 boards to build the connection.After I se...

Client of Generic On/Off, Sensor Model

I found that I can make vendor model client with BluenrgMesh_SetRemoteData(), BluenrgMesh_ReadRemoteData() functions using BlueNRG embedded SDK.However, these functions looks only for vendor models. Are there any APIs to make standard models client l...

SKimu by Associate II
  • 1020 Views
  • 2 replies
  • 0 kudos

S2LP and AFC_CORR register to get frequency offset.

After receiving a package I read out the AFC_CORR register. This value is not very stable, even if packages comes from the same sender.So I have 2 questions:How do I get the frequency offset in Hz from this register?Why is this not stable.best regard...

aritec by Associate III
  • 532 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.