Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLUENRG-2 - Change Adversitive Interval

Hi! I developed pcb with BLUENRG-2 IC. Where in BLE-Beacon example (ST BlueNRG-1_2 DK 3.1.0) I may change Adversitive Interval? This is need for me, because my application need more free CPU time. Thank you!

rraf3 by Associate
  • 705 Views
  • 0 replies
  • 0 kudos

High current consumption in S2-LP

I'm using Bluenrg232 and S2-LP to send sigfox messages. I noticed that the current will spike from 5mA to 125mA to sending sigfox message. The specifications of S2-LP shows that the current consumption for TX is 10mA. is there something wrong with my...

CChon.0 by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

X-CUBE-BLE1 drivers usage in new project

Posted on June 02, 2018 at 17:29Hello,I am working with the X-NUCLEO-IDB05A1 BLE expansion board on the NUCLEO-L476RG board and I want to send sampled ADC values via Bluetooth LE. Software I use: STM32CubeMX V4.25.0, SystemWorkbench for STM32.I succ...

BlueNRG2 programing

Hi,I have STEVAL-IDB008V2 and I would like to start develop something on BlueNRG2 SoC which is on this board. I am looking for some tutorials or manuals for this device. On the Internet is nothing about this, only for using BLE as external device. I ...

voucher displayed using terraterm demo board P-L496G-CELL 02 Board showing "Wrong voucher code" when tried https://stm32-c2c.com/sim/en/boards/dashboard please provide me valid voucher?

voucher displayed using terraterm demo board P-L496G-CELL 02 Board showing "Wrong voucher code" when tried https://stm32-c2c.com/sim/en/boards/dashboard please provide me valid voucher?

DPADI.19 by Associate II
  • 1298 Views
  • 2 replies
  • 0 kudos

Connect X-NUCLEO-IDB05A1 to PC

I'm trying to connect an X-NUCLEO-IDB05A1 (connected to a Nucleo-F411RE) to my PC... eventually I am going to be connecting to another IDB05A1 device, but I figure it is easier to try to get the basics going when I am only writing code on one side of...

DSabo by Associate III
  • 741 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.