Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-MS How to fix unhandled event 16

Hi, I'm using NUCLEO-F401RE+X-NUCLEO-IDB05A1 as a central.After start scan, I got unhandled event 16.Is 16 = EVT_BLUE_GAP_ADDR_NOT_RESOLVED_BIT?How should i fix it? or what may i set wrong?Bluetooth firmware is bluenrg_7_2_c_Mode_2-16MHz-XO32K_4Mand...

KHuan.9 by Associate
  • 733 Views
  • 0 replies
  • 0 kudos

How to configure the STWINK to be able to connect to multiple devices via Bluetooth at the same time?

When my Raspberry Pi with BLUEST-SDK-PYTHON is connecting to the STWINKT, my Android Phone with ST BLE Sensor app cannot connect to it and When my Android Phone is connect to STWINKT, my Raspberry PI cannot discover or connect into it (I am using ex...

reokyouma by Associate III
  • 708 Views
  • 0 replies
  • 0 kudos

My P-l496G-CELL02 C2C device won't connect.

Using the google cloud platform, have connected via the STLINK, have configured the modem using the binary file provided for google cloud platform. Using an NBIOT external sim card but when the APN is set for C2C capability, the response on the termi...

JGood by Associate II
  • 2143 Views
  • 3 replies
  • 1 kudos

How do I configure the STUSB4500 as a PPS sink?

Using an Aukey PA-Y10 supply with the STUSB4500 works fine for all the five fixed-voltage PDOs (5V, 9V, 12V, 15V and 20V).However, the supply's manual says that it features a PPS output with 3 to 16V but I found no way to access this with the STUSB45...

MForw by Associate
  • 1541 Views
  • 2 replies
  • 0 kudos

Steval-FKI433V2 & SDK_Chat example: how to increase a Communication range?

I use SDK_Chat example (S2LP DK1.2.1\..\S2LPLibrary_Examples) as a base for my project.To increase a Communication range I change next parameters:DATARATE                   38400 (default) to 4800POWER_DBM                  12 (default) to 14RSSI T...

bvn123 by Associate II
  • 607 Views
  • 0 replies
  • 0 kudos

Where to find ST7540 DEMOKIT GUI?

Hi all,I recovered 2 old ST7540 DEMOKITs complete of the related ST7-based COMMBOARDs (photo attached); however I don't have the DEMOKIT GUI that is cited in the UM0239 I found on the ST website (https://www.st.com/en/interfaces-and-transceivers/st75...

BlueNRG-2 VBAT max rating

Hi,I'm designing a beacon around the BlueNRG-2 and would like to power it from a battery that can output as much as 3.67V. Unfortunately this exceeds the max Vin limit on the datasheet (3.6V) by only 70mV. I have a couple of questions in the hopes of...

jaylong by Associate II
  • 596 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.