Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2LP : Impossible to write registers

We've been using the S2LP in several designs, and we are happy with it. I'm working on a new PCB. However, since two days, I'm stuck with bug I have no more ideas how to debug it.I can read the registers successfully, but whenever I try to modify one...

VCano.1 by Associate
  • 830 Views
  • 1 replies
  • 1 kudos

Hello, We have developed a board using BLUENRG-232. While we upload the example code, we are not getting Bluetooth detected.

We uploaded the BlueNRG-2 chat example code to our custom board.We got the expected output in the terminal window .But the Bluetooth is not available in any Bluetooth app.I'm attaching the screenshot of the output obtained from serial terminal.Could ...

0693W000001sKuBQAU.jpg
MMANU.1 by Associate
  • 696 Views
  • 0 replies
  • 0 kudos

Connecting BLUENRG-M2SA to a Raspberry Pi

Hi,I want to conenct the BLUENRG-M2SA to a Raspberry Pi. This needs to be done through the USB connector.Can I use a USB-to-UART IC to connect to the UART pins of the BLUENRG-M2SA and then flash the software using this?Also, do I need to connect the ...

Looking for solar charger IC with following specs... 1.Input voltage of IC - min -5v and max -22v 2.Charging current - min 800mA 3.IC output voltage - 4.2V 4.Should be configured with MPPT technique.

Looking for solar charger IC with following specs...1.Input voltage of IC - min -5v and max -22v2.Charging current - min 800mA3.IC output voltage - 4.2V4.Should be configured with MPPT technique.

Jm.11 by Associate
  • 792 Views
  • 0 replies
  • 0 kudos

IOS ST BLE Apps not able to connect to F401RE+IDB05A1. It shows 'Connection Timedout'. May I know what might be the reason? It works with Android

- The .bin sample is from https://os.mbed.com/teams/mbed-os-examples/code/mbed-os-example-ble-HeartRate/- The (iPhone) IOS Software version is 13.5.1, while the iPAD IOS Software version is 13.3-The timeout time capture around 10s from 'connect' clic...

0693W000001sAu1QAE.jpg
MAb H.1 by Associate
  • 695 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.