Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-M2SP vs M2SA

In the datasheet of the BLUNERG-M2 module, it states the following:"The BlueNRG-M2 module allows applications to meet the tight advisable peak current requirements imposed withthe use of standard coin cell batteries. Optimized results are obtained wh...

stevang by Associate
  • 1162 Views
  • 1 replies
  • 0 kudos

L9663 PSI5 communication inquiry

I want to communicate with ECU using L9663 PSI5 transceiverUse only transmission mode, No receiving mode is required.In the circuit diagram in the datasheet, it looks like PSI1 and 2 pins are connected to the ECU. Is that right?What is the DOUT pin? ...

yjpark by Associate
  • 560 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.