Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP SMPS

Admittedly, this is going to be a challenge to answer since it appears what I'm doing is against the specification... but here it goes... hopefully someone at ST knows...Are most folks using these radios only in battery applications? I ask because t...

JMath.2 by Associate II
  • 1205 Views
  • 0 replies
  • 1 kudos

WB5x: HCI bugs over UART transport

Hi All,There seems to be multiple bugs in the HCI implementation for WB series chips.Are there any newer builds of this image where these are fixed?Setup: Using reference dongle from P-NUCLEO-WB55.stm32wb5x_FUS_fw.bin latest version - 1.1.2stm32wb5x_...

donpedro by Associate II
  • 2635 Views
  • 4 replies
  • 0 kudos

Can't load code on STEVAL-IDB011V1 by Keil

Hello.I'm using STEVAL-IDB011V1. From the BlueNRG-LP Navigator, I can load the examples on the board. But when I'm using the Keil, it says "SWD/JTAG Communication Failure".On the options for target in the tab "Device" the device is BlueNRG-355, and t...

Resolved! BlueNRG-2 maximum SPI clock

I am currently using a X-NUCLEO-BNRG2A1 to experiment with the BlueNRG-2. I initially set the SPI rate to 1.25 Mbit/s, but later noticed in the BlueNRG-2 documentation that the maximum SPI rate is 1Mbit/s. My question is how strict is this SPI rate l...

BPaik by Senior
  • 1827 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.