Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi everyone! I am trying to interface my TETRA device with the microcontroller using the USB interface. The microcontroller will act as a usb host while the TETRA will act as a USB device. I am using STM32F469I-DISCO development board.

How can I do such kind of interfacing. Also note , this TETRA device needs a specific USB driver to install and run while connecting with the PC windows. Does the development board can support only those usb devices which don't need a driver run?

SMuha.3 by Associate
  • 799 Views
  • 0 replies
  • 1 kudos

We want to use the S2-LPQTR for proprietary protocols. Therefore we need external control of the TX- and RX-mode of the transceiver. We intend to do this over GPIO 0 and 1, as short mentioned in the datasheet, page 65, table 61.

Do you have a typical schematic or an application note that deals with such a setup, to have direct hardware control of the TX- and RX-mode, and also to access the TX and RX data in a very direct way?In our application the TX/RX time and RX/TX time i...

HOppl.1 by Associate
  • 674 Views
  • 0 replies
  • 0 kudos

What is the difference between device versions C1 and 91 of S2LP (DEVICE_INFO0) ? Is it any silicon level change or firmware level change?

Is there any silicon level change in S2LP devices with device versions C1 and 91 since we observed there is difference in current consumption in standby mode. 91 is draws 29µA and C1 is drawing < 1µAWhat is the difference between device versions C1 a...

SMall.2 by Associate
  • 867 Views
  • 1 replies
  • 0 kudos

ST-Link V3 works well with BlueNRG2 when used from IDE like Keil uVision, but fails in BlueNRG1 ST-Link Utility

Hello,I've started to suspect that something is not quite right with the BlueNRG-1 ST-Link Utility. I have a ST-Link V3 connected to STEVAL-IDB008V1M. I can flash and debug the module from Keil uVision5, but when I try to flash the module from BlueNR...

JLepi.1 by Associate II
  • 2953 Views
  • 2 replies
  • 1 kudos

STUSB4500 PDO profile doesn't change after setting.

Hi,Through some setup, I was able to access STUSB4500 using the GUI tool in STSW-STUSB002.After I set the second profile to 20V/5A, I connected a power supply with 5V/3A and 20V/3.25A PDO capability. But nothing changes and the voltage is unchanged a...

0693W000008wLMzQAM.png
BHan.1 by Associate II
  • 6572 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.