Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIV3F's input Vcc_io gets randomly tied to gnd

Hi everybody,I have been using for a while liv3f product and, before creating the schematics i read carefully the hardware manual and the electrical caracteristics.Once I have put it on a pcb, it was working well and i was getting gps signals. But af...

ABouk.1 by Associate III
  • 754 Views
  • 0 replies
  • 0 kudos

Is it possible to switch between ASK modulation and unmodulated CW in S2LP without having to restart the Tx mode?

I am using the S2LP Tx module for transmitting data with ASK modulation. After the end of the data, I want to transmit CW continiusoly. I see that one can change the register settings to switch between ASK and unmodulated (CW) mode. But my question i...

NAwari by Associate II
  • 929 Views
  • 0 replies
  • 0 kudos

BlueNRG-MS Read Device Name of Central Device

I have a peripheral BlueNRG-MS device where a mobile phone is connecting to, what is to right function to use to get the device name of the mobile phone? My understanding is that I have to use some GATT service... but I can't figure out how the get t...

aj.sk by Associate III
  • 839 Views
  • 0 replies
  • 0 kudos

BlueNRG ACI protocol

Is there a document describing the bluenrg ACI protocol ? I intend to connect a windows computer to a X-NUCLEO-BNRG2A1 via UART, and use the default DTM firmware to do some basic evaluations.I can see these possibilities:reverse-engineer BlueNRG-1_2 ...

ELema by Associate
  • 867 Views
  • 0 replies
  • 2 kudos

Resolved! S2-LP: outdated sources for CLI

Hi,Binaries provided in S2-LP Development Kit v.1.3.3 (en.stsw-s2lp-dk_firmware) are newest than sources provided in that package:Binaries version: 2.3.3Source code: 2.3.0Please provide the sources that were build to that binaries (this ask is direct...

I am looking for reference circuit designs for the spirit1 low power sub-GHz transceiver. The data sheet is limited and the design references is no longer on ST. Does anyone have more information about layout and setup?

I have found modules for 433MHz band but I need to design a circuit for ~169MHz (VHF band).I'm unsure of the matching circuit and which components to use.Any help would be greatly appreciated.

SJeff.1 by Associate II
  • 1120 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.