Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M41T62 RTC Alarm

Hello, We are currently using the M41T62 RTC which is connected to a STWINKT1B board from ST along with the drivers meant to be used with M41T62(download page).We have been successfully able to use it to set a 1 min alarm with interruptions in repeti...

Where can I finfd the SPWF01S firmare packages STSW-WIFI001? I need to upgade the firmware of the X-NUCLEO-IDW01M1 expansion board

Hello, I'm trying to upgrade the firware of the SPWF01S. In the upgrading manual it's says that I need a binary file to program the flash. I saw that the package was avaible in the following link, but now that page doesn't exists. From where can I do...

Javi by Associate
  • 1091 Views
  • 1 replies
  • 2 kudos

Unable to connect to board using Unico GUI

I have 6 of these dev boards. one of them i bought before the other 5. for the later one the STEVAL -MKI205V1 dev board I'm trying to test is returning a "ERROR: The adapter board has not been recognized, the WHO_AM_I register value does not match th...

0693W00000D1f0kQAB.png
YFels.1 by Associate
  • 879 Views
  • 0 replies
  • 0 kudos

Cannot load new program to my board

I am working with the BlueNRG-M2SA evaluation board and I am using the ST-Link / V2 to load program on the board,I managed to load my first program on the board. But I can no longer load a new one.When I load a new program onto the board, the old pro...

COlva.1 by Associate II
  • 970 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.