Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3MODS use the VCP

Hi everyone,I see there are differences between V3MODS und V3MINI in the assembly, jumpers etc.Do I need to assemble any jumpers to make the V3MODS VCP run on CN2 Connector?Best regards,Mathias Brandl

mathias by Associate II
  • 1011 Views
  • 1 replies
  • 0 kudos

Resolved! BlueNRG2 OTA Flash verify failure

HelloI'm trying to implement the OTA feature in my project. We use the BlueNRG-2 Chip.I'm followed the BLE_Chat example and the explanaition in the The BlueNRG-LP (over-the-air) firmware upgrade document to inlcude all the ota related code parts.When...

TGats.2 by Associate II
  • 2855 Views
  • 5 replies
  • 1 kudos

BlueNRG-X Flasher Utility (4.1.0) is not recognizing SWD connections when ST-link/V2 is connected. I'm running the flasher through a command line interface to get the error message (BlueNRG-X_Flasher_Launcher.exe).

The error message that appears is:"Traceback (most recent call last): File "Script_launcher.py", line 542, in <module> File "globals.py", line 555, in get_stlink_list File "build\bdist.win32\egg\usb\core.py", line 1246, in device_iter File "build...

0693W00000D1efmQAB.png
VLima.1 by Associate II
  • 3457 Views
  • 5 replies
  • 0 kudos

Measuring the reliability of mesh network

I want to measure the reliability of bluetooth mesh network. I am using two STEVAL-IDB008V2 boards , one STEVAL-IDB007V1 board and an android smartphone to construct a bluetooth mesh network and using the lighting demo project of STSW-BNRG-Mesh v 1.0...

MH1 by Associate II
  • 4511 Views
  • 7 replies
  • 0 kudos

S2-LP GUI base frequency and Synth value

Dear,having started 2 S2-LP evaluation boards and setting the base frequency in the GUI to 915 MHz. 1ste S2-LP calculates 914.999.999 Hz and second one calculates 915.000.004 Hz with corresponding Synth register values 0x02 0x49 0x98 0xF8 hex and 0x...

PPelg.1 by Associate
  • 801 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.