Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connection with ST25PC-NFC and M24SR.

Hi, I check connection with ST25PC-NFC and M24SR.I used the NDEF Editor of ST25PC-NFC.The error occurred error after selected "Read from your tag".This error is "Read tag operation failed!". Please take care my trouble.

0693W00000Kbm8WQAR.jpg
Haru by Associate II
  • 585 Views
  • 0 replies
  • 0 kudos

ST BLUENRG-LP Bluetooth as a slave machine, how to forbid the other host to initiate the pairing request, I want to only allow the slave machine to initiate the pairing request

ret = aci_gap_set_io_capability(IO_CAP_NO_INPUT_NO_OUTPUT);ret = aci_gap_set_authentication_requirement(BONDING, MITM_PROTECTION_NOT_REQUIRED, SC_IS_SUPPORTED, KEYPRESS_IS_NOT_SUPPORTED, MIN_KEY_SIZE,  MAX_KEY_...

Fx.1 by Associate II
  • 828 Views
  • 0 replies
  • 0 kudos

Resolved! hi, I refer to demo"BLE_Security" in BlueNRG-LP , meet this error , API "aci_gap_set_authentication_requirement " return 0x11 err; #define BLE_ERROR_UNSUPPORTED_FEATURE ((tBleStatus)(0x11)) why?

code:void test_security_init(void) {   Clear_Security_Database(); int ret; /* ACI_GAP_SET_IO_CAPABILITY */ ret = aci_gap_set_io_capability(IO_CAPABILITY); if (ret != BLE_STATUS_SUCCESS) { TUYA_APP_LOG_INFO("aci_gap_set_io_capability(%d...

Fx.1 by Associate II
  • 2536 Views
  • 4 replies
  • 0 kudos

DTM does not build for BlueNRG-345

We are doing FCC and BQB approval next week and I am trying to build the DTM project for the BlueNRG-345 and have the requisite defines for C/C++ and linker but it runs out of RAM on the build.Please explain and point me to the correct changes needed

RAdam.1 by Associate III
  • 1191 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.