Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wise-studio on macOS ARM64

Hey,I am trying to develop firmware for a BLUE-NRG module using Wise-studio, I have done this before on a Windows machine.Now I am trying to install Wise-studio on a MacBook M4 Pro, which is Apple silicon.I downloaded the .dmg and installed it, and g...

Resolved! ST87M01 - LTE-M Support

Hi, I have been looking at this newer ST87M01 as of here :- https://www.st.com/resource/en/datasheet/st87m01.pdf and wondered does it support LTE-M or only NB-IOT? Thanks!

Link_P by Associate
  • 396 Views
  • 3 replies
  • 1 kudos

L9780 - SPI communication issue

All,I'm working on the basics of getting the SPI communication set up for the L9780 IC and am running into some issues, so I'd appreciate some feedback or a double-check. It appears so far that I'm able to send a command via the control word and succ...

Resolved! Problem with ST67W61 in w61_at_common.c

Greetings,I'm trying to run an application using X-CUBE-ST67W61, but I'm encountering a problem at this line in w61_at_common.c: int32_t W61_AT_ModemInit(W61_Object_t *Obj) { (...) xReturned = xSemaphoreTake(mdm->sem_if_ready, pdMS_TO_TICKS(4000)); (...

Shirovaty_0-1765976870783.png
Shirovaty by Associate II
  • 1289 Views
  • 6 replies
  • 2 kudos

Resolved! ST KNX 68R Immunity Test Problem

We are using 2 KNX IC on our project. One of them for communication and some LEDs other one (STKNX) just for driving LEDs not for communication. But of course is directly connected to KNX_BUS line. When we applied Surge test , TVS couldn't protect th...

Resolved! QoS configuration on ST67W

Hi, i have bought a Nucleo-U575ZI-Q coupled with a X-Nucleo-67W61M1 i have upload the exemple ST67W6X_MQTT, after reading the doc i have complete the configuration and i run well.  I use it with mosquitto or nanomq brokers (same results) but on both ...

XP_LGE by Associate
  • 1094 Views
  • 2 replies
  • 0 kudos

Stpm34 spi not connecting

i have a problem that has bugged me for a while now. Im using a stm32f4 microcontoler to read data from stpm34 microchip, but i can not establish a spi connection betwen them. With my logic analyzer i can see that i send mosi, the clock works and i b...

Robi123 by Associate
  • 275 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.