2017-01-06 11:54 PM
The function aci_gatt_update_char_value fails initially....and if fails there is while(1) loop...so system stuck here....what is issue ? after debugging it observed that function returns BLE_STATUS_TIMEOUT.....can you suggest solution for issue
2017-01-09 1:50 AM
Hello
We have forums setup to ask questions which you can see from the forums menu at the top of this page. Which ST product are you working with?
Thanks
2017-01-09 2:55 AM
We are using Bluetooth module BlueNRG-MS
2017-01-09 4:11 AM
Could you look at the list of options in the Forums menu and let me know which option is the correct one? E.g.
or , thanks.2017-01-09 4:23 AM
INTERFACE AND CONNECTIVITY ICS
2017-01-09 4:39 AM
I have moved this thread to
. , orGallucci.Gerardo
can you help with this question or tag someone who could?Thanks
2017-01-10 3:05 AM
I replied to this question here:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.