2022-02-21 7:24 AM
I noticed that an5471 says that the uart interface for flashing the bootloader is only available on PA8 and PA9, but those pins aren't present on the 32 pin version. Is there any other way to access the bootloader on this device?
Solved! Go to Solution.
2022-02-21 8:29 AM
Welcome, @RMcCa.3, to the community!
As you can find in the datasheet, the UART is also available on the QFN32, namely PA8 = pin 8 and PA9 = pin 7.
Does it answer your question?
Regards
/Peter
2022-02-21 8:29 AM
Welcome, @RMcCa.3, to the community!
As you can find in the datasheet, the UART is also available on the QFN32, namely PA8 = pin 8 and PA9 = pin 7.
Does it answer your question?
Regards
/Peter
2022-02-21 8:38 AM
Thank you, I must have mixed up PA and PB when I was reading it before. Does it matter that uart isn't listed on those pins in the datasheet? It has usart instead for af0 for both pins.
2022-02-22 12:53 AM
No, it does not matter because UART is only a partial function of an USART and thus an alternative designation.
When the bootloader is activated, it configures the two pins PA8 and PA9 to use them as UART.
Good luck!
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.