2020-12-10 7:24 AM
If I want to take multiple readings on a VL53L1X at different ROI's, I need to set the optical centers for each ROI sequentially, one for each measurement.
But when exactly do I do that, and what are the pitfalls?
e.g. I have a timing budget of 20ms, and an inter-measurement period of 25ms (so 5ms gap between measurements).
Then I start ranging on the sensor.
Thanks!
Solved! Go to Solution.
2020-12-10 7:38 AM
2020-12-10 7:38 AM
2020-12-10 7:41 AM
You might also consider not setting an IM period and using a 25ms timing budget. It gives you a more accurate answer at the same timing. Does use a bit more power though. Not settting an IM period just means a new one will start immediately after the prior one finishes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.