2019-06-11 5:06 PM
On our prototype circuit boards with VL6180x sensors there are 6 sensors per board. On a couple of our prototype boards (about 10% of our boards) we have seen just a single sensor able to respond over I2C but cannot start ranging. The result range status register always reports a result__range_error_code: 1 - VCSEL Continuity Test error. I2C communications are fine and all other 5 sensors are able to range.
What is this power up test doing and what could cause this error?
2019-06-24 9:44 AM
It's a power issue.
The ToF chips from ST use 20mA when they are running. But that is an average during the 10ms or so it takes to get a range.
At the micro level the laser turns on and off at about a 30% duty cycle and during that 'on' the sensor draws quite a bit of power.
We believe this is your issue.
Bigger regulator perhaps?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.