2023-11-21 7:51 PM
Hi guys, I'm using vl53l7cx without cover glass.
I use the Example_1_ranging_basic in VL53LMZ_ULD_API driver, but i alway receive the result with target_status 6 and the result's distance_mm seem not correct.
Eg i put an target about 300mm in front of the sensor and get result as below in resolution 4x4:
1168-6, 1348-6, 1302-6, 1243-6
1213-6, 1371-6, 1330-6, 1249-6
1240-6, 1381-6, 1332-6, 1253-6
1215-6, 1360-6, 1317-6, 1248-6
So i wonder if i miss any config to get the correct ranging result?
Thanks.
Solved! Go to Solution.
2023-11-22 2:40 AM
Status 6 is RANGECOMPLETE_NO_WRAP_CHECK
So first question is : the data you are showing are from the first frame received or not ?.
Then .. suspicious that the ranges you record are about 4x the expected value….which just so happens to be the ratio that the raw data is adjusted by depending on this define in the platform.h file…
/*
* @brief The macro below can be used to avoid data conversion into the driver.
* By default there is a conversion between firmware and user data. Using this macro
* allows to use the firmware format instead of user format. The firmware format allows
* an increased precision.
*/
//#define VL53LMZ_USE_RAW_FORMAT
Is this parameter defined ? If yes, you would see target ranges 4x larger than they expect.
2023-11-21 11:19 PM
Hello,
Can you please give more details about your use-case ?
Which hardware are you using ? Is it a ST EVK or your own PCB board ?
You are mentioning the VL53L7CX and the VL53LMZ_ULD_API driver used for VL53L7CH.
Regards
Anne
2023-11-21 11:46 PM
2023-11-21 11:51 PM
Hi @Anne BIGOT this is the device info when i get from the chip:
- device id: 240
- revision id: 2
- module id: 1
2023-11-22 2:40 AM
Status 6 is RANGECOMPLETE_NO_WRAP_CHECK
So first question is : the data you are showing are from the first frame received or not ?.
Then .. suspicious that the ranges you record are about 4x the expected value….which just so happens to be the ratio that the raw data is adjusted by depending on this define in the platform.h file…
/*
* @brief The macro below can be used to avoid data conversion into the driver.
* By default there is a conversion between firmware and user data. Using this macro
* allows to use the firmware format instead of user format. The firmware format allows
* an increased precision.
*/
//#define VL53LMZ_USE_RAW_FORMAT
Is this parameter defined ? If yes, you would see target ranges 4x larger than they expect.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.