2024-07-09 2:01 AM
Is the VL53L7CH software (STSW-IMG043_ULD) a superset of the VL53L7CX (STSW-IMG036) software? That is, can I use the VL53L7CH software with both devices?
Best,
Anton
Solved! Go to Solution.
2024-07-09 5:35 AM
If we have a superset board, we don't have a superset SW
So if you want to test the VL53L7CX you have to use its specific SW package STSW-IMG036.
2024-07-09 5:35 AM
If we have a superset board, we don't have a superset SW
So if you want to test the VL53L7CX you have to use its specific SW package STSW-IMG036.
2024-07-09 7:09 AM
I see. I seem to be able to run the VL53L7CX with the software for the VL53L7CH though (of course without using the CNH capabilities). I'm running the "basic ranging" example.
Anyway, I suppose it does not matter much. I can have both software packages side by side if need be. Thank you for answering.
2024-07-10 2:22 AM
Indeed, it can work but you have to keep in mind that ST is guaranteeing only the SW/HW package delivered.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.