2021-04-26 9:15 PM
Hi,
I am planning to use VL53L1X ULD API for calibration functionality. Host system is Raspberry PI and I got source code of VL53L1X ULD and Example Application from https://my.st.com/content/my_st_com/en/products/embedded-software/imaging-software/stsw-
2021-04-28 7:08 AM
l double-checked. There is a makefile in there. In fact there are two.
If you want to use interrupts, you need a kernel module to absorb the interrupt and then make a call-back for you.
That code is in there - but you only need it if you want to use the interrupts. Otherwise the code will poll for done.
I'd start with the polling-type program until you are confident it works and then move on to the interrupt.
The code is simple and hopefully straight forward.
Good luck.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.