2020-03-06 2:09 AM
I want to use multiple VL53L1x sensor with same I2c bus so can we change sensors address
2020-03-06 2:56 AM
Hi,
You may check out the guide made for the VL53L0X AN4846: Using multiple VL53L0X in a single design from ST.COM. The same principle is applicable for the VL53L1X.
Thanks,
Julien
2020-03-06 8:02 AM
I don't want to disparage an ST document, but that one goes a little far.
Here is what you do:
Attach each sensor's 'shutdown' pin to GPIO's on your host.
At boot, put them all in reset.
Bring them out one at a time.
Use the Address Change I2C command to change the addresses.
Repeat for each chip.
And even though it's not strictly required, consider changing the address for all the sensors - even the last one.
That way if you ever get a glitch and a sensor resets, it will start responding on the initial address.
2020-05-22 3:28 AM
thanks sir
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.