cancel
Showing results for 
Search instead for 
Did you mean: 

Calibration: Is it necessary if only the change in distance is the important value?

videojames
Associate III

In our application, we don't necessarily need to know the true distance, we only need to know when it's in a certain range, and it doesn't matter if that range is represented as 30-40mm or 50-60mm, only that is consistent.

Can we get away with not needing calibration if this is the case?

We are using a VL53L1X aimed through a IR transparent plastic.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
John E KVAM
ST Employee

I think it depends. If you build your system with a thin, clear, optically flat glass near to the sensor, then no, the effect of the crosstalk will not significantly affect your range at that distance.

But be a little careful. If you choose a big air gap between sensor and the glass, or the glass is of poor quality, then you could be in trouble.

The final determination of the quality of glass would be the calibration return. But with this sensor, if it works for you, it works. But the build-it-and-see-if-it-works can be expensive.

Buy the P-Nucleo-53L evaluation kit and test the glass you are using at your expected air gap. It will save you a lot of money in the long run.

Read and understand the article at:

https://community.st.com/s/article/Time-of-Flight-Cover-glass

And you will be fine.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.

View solution in original post

1 REPLY 1
John E KVAM
ST Employee

I think it depends. If you build your system with a thin, clear, optically flat glass near to the sensor, then no, the effect of the crosstalk will not significantly affect your range at that distance.

But be a little careful. If you choose a big air gap between sensor and the glass, or the glass is of poor quality, then you could be in trouble.

The final determination of the quality of glass would be the calibration return. But with this sensor, if it works for you, it works. But the build-it-and-see-if-it-works can be expensive.

Buy the P-Nucleo-53L evaluation kit and test the glass you are using at your expected air gap. It will save you a lot of money in the long run.

Read and understand the article at:

https://community.st.com/s/article/Time-of-Flight-Cover-glass

And you will be fine.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.