Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reduce noise when targeting reflective curved surface

Hi, We are trying to measure distance from our sensor through an IR Translucent plastic to a curved metal surface, using a VL53L1X. We are getting reasonable results by they are rather noisy (~10% deviation at times)What sort of changes should we be ...

Resolved! VL53L5CX gasket requirements with cover window and large air gap

As exposed in the Application Note AN5231 of the VL53L1CX, a gasket may be required to limit the negative crosstalk effect if a cover window and a large air gap were both present. Is there any similar Application Note specific for the VL53L5CX model?...

0693W00000Kb9GRQAZ.png
MFabb.1 by Associate II
  • 1995 Views
  • 2 replies
  • 0 kudos

Resolved! how to calibration 6180

hi,stI am using a 6180 to measure the height of milk. The height of vl6180 from the milk is about 10 - 60mm,anf the front of the sensor is covered with a layer of clear plastic. I don't know how to do the offset calibration.1. Remove the covering pla...

Zwf.1 by Associate II
  • 6918 Views
  • 17 replies
  • 0 kudos

Query regarding VL53L1CB data depicted on it's website

Under "All features" information, the following data is depicted:"400 cm+ detection with full field of view (FoV)60 Hz ranging capable up to 300 cm"In datasheet it's written, the sensor can measure up to 8m. However, this "60 Hz ranging capable up to...

SA.13 by Associate
  • 1034 Views
  • 1 replies
  • 0 kudos