Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! About the dead time of VL53L8CH

I woulke to know the dead time of VL53L8CH to know the max value of one bin, but there is no information in the datasheet. Besides, currently I am using  the example in VL53LMZ_MassMarket_ULD of cubeide to get the histogram, I want to know if the num...

Licx by Associate III
  • 2312 Views
  • 2 replies
  • 0 kudos

Resolved! ID Register to differentiate VL53L0x, VL53L1x, etc

Hello!   I am working on a project where I would like to be able to detect which type of sensor I have connected (via I2C). For example, I am currentky planning on using a VL53L0x, but would like to be able to detect on boot if I am still using the V...

mttdarko by Associate II
  • 2666 Views
  • 4 replies
  • 4 kudos

Resolved! lens for receiver side of vl53l4cd

I need to measure a distance within a 1 degree field of view (FOV) in front of the sensor at a distance well within the range of the sensor. I know I can't use focusing optics on the emitter side without changing the laser class - so I won't. Using a...

Resolved! Replacement for VL6180X - what type is recomended -

Hi,i saw that the VL6180X is set to NRND.I need the functions of gesture detection and ambiation light measurement.I want to use it in a new product which should be produced more than 10 years but in this case i dont think that this is the right one....

Joetech by Associate
  • 2184 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L4CX Difference between the two modes of offset

Hi,I would like to ask about the difference between the two modes of offset (PerformOffsetSimpleCalibration and PerformOffsetPerVCSELCalibration).Because when the crosstalk calibration value is high(calibrationData.customer.algo_crosstalk_compensatio...

sctz by Associate III
  • 2490 Views
  • 4 replies
  • 0 kudos

Resolved! vl53l0x sensor detection distance inquiry

(A translator was used for this inquiry.)Hi,I am using the vl53l0x sensor.I would like to inquire about the detection range of the sensor.What value do you get when the wall you want to measure the distance against is tilted? (Refer to image1)What po...

pcbsmt by Associate II
  • 3318 Views
  • 3 replies
  • 0 kudos

I2C not working properly with sequencer. Why?

Hello guys,Im trying to learn about LoRa and else. Now, I am using an SubGHZ_Phy in stm32wl sdk. The problem is, when I am using vl6180x codes in while loop without sequencer, it does work! But, When I am trying to implement it with a 5 min util time...

Can't run VL6180x properly with seauencer, why?

Hello guys,Im trying to learn about LoRa and else. Now, I am using an SubGHZ_Phy in stm32wl sdk. The problem is, when I am using vl6180x codes in while loop without sequencer, it does work! But, When I am trying to implement it with a 5 min util time...

Javidx9 by Associate
  • 1386 Views
  • 0 replies
  • 0 kudos

Resolved! What do you think about not responding of the sensor after resetting or unplugging enp8266 nodemcu v

 Hi how are you …i bought a new esp8266 (also I bought logic level shifter and 74125 IC) and built the project from the beginning as the schematics in the beginning it works fine the rgb ring lights up and the sensor responds and performs the interru...

Screenshot (5).png