2024-04-17 10:19 PM
(A translator was used for this inquiry.)
Hi,
I am using the vl53l0x sensor.
I would like to inquire about the detection range of the sensor.
Thank you.
Solved! Go to Solution.
2024-04-19 9:15 AM
The cone of light - or it' Field of View is 27 degrees.
With a little trig one sees that the diameter of the illumination circle is 1/2 the distance.
The astute reader will do the math and get 0.44 but it's a question of accuracy.
Very near the sensor the FoV is wider, and it narrows as the distance increases.
So, go with 1/2 and you will be as good as you are going to get.
- john
2024-04-18 7:45 AM
In the first image when you have a slanted wall, you will get the average of all photon return times.
The trouble is that near objects return more photons than a far object. So instead of the mathematical average, you will see a number weighted toward the closer distance.
Unfortunately, how much of this effect you see will depend on the reflectivity of the wall.
As far as a wall at 2M what you get will depend on the reflectivity of the wall. If it's bright enough to return photons you will get 2M and status =0. A less reflective will will give you Staus =2 (low signal). With a REALLY bright target, beyond 4M you will get a status 4. Status 4 means you have a wrap around issue. Wrap-around (also called Aliasing) is a condition where the photons from pulse A get returned after the pulse of pulse A+1. So with a bright wall beyond 4M, you get a Range Status =4 and the correct distance minus the 2M wrap around point.
If this bothers you, a pin-compatible part (VL53L3CX) is available. It's an L0 part with better mathematics.
2024-04-18 6:05 PM
Thank you for your kind reply.
Regarding question 2, I am curious about the detectable area.
The sensor's detection range appears to be gradually expanding in a cone shape.
Then, I would like to know the area of the detectable area from a distance of 2M.
(Part marked with a question mark in Image 2)
Thank you.
2024-04-19 9:15 AM
The cone of light - or it' Field of View is 27 degrees.
With a little trig one sees that the diameter of the illumination circle is 1/2 the distance.
The astute reader will do the math and get 0.44 but it's a question of accuracy.
Very near the sensor the FoV is wider, and it narrows as the distance increases.
So, go with 1/2 and you will be as good as you are going to get.
- john
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.