Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5/L7CX target status validity

Hello,the VL53L5CX and L7CX ULD guides mention that a target status of 6 and 9 should be considered with a confidence of 50 %, while a comment in the api.h file says that  "5 & 9 means ranging OK", which gives the impression of a higher confidence ra...

lukaskn by Associate II
  • 1648 Views
  • 1 replies
  • 0 kudos

Resolved! How exactly do I read the histogram on VL53L8CH

Hello Community, I am new here and new to this field as well. I am currently using the VL53L8CH Lidar Sensor which has a MZAI some GUI tool to access and save data logs along with some visualizations of the data.I am currently doing some experimentat...

koch by Associate II
  • 2629 Views
  • 2 replies
  • 1 kudos

Resolved! Calibration card

Calibration of ToF sensors requires a target which is '17% reflective'. Can I take it this means a simple peice of paper or card printed on a laser printer at 83% black (greyscale)?Thanks

Resolved! Wait for sensor booted fails

I was using the sensor until now on an Raspberry Pi with direct access to the I2C bus without problems.Now I use an FT260 USB-I2C interface to communicate to the sensor from a PC via USB. In principle the communication is working, e.g. vl53l5cx_is_al...

PBoer.1 by Associate II
  • 2742 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CX / CD Calibration

Hi there,  I am using multiple VL53L4CX sensors and the target is a person's hand within a 60cm range. I am wondering if there is a specific calibration method for a hand within a shorter range (60cm), to improve readings. Right now I am just using t...

isaacjack by Associate II
  • 1728 Views
  • 1 replies
  • 0 kudos

vl53l5cx_check_data_ready returns C5 GO2 error

I was able to run the vl53l5cx demo, however when calling 53l5cx_check_data_ready, I see that it reported a 'GO2'error. The code is C5.The content of the (relevant?) config.tempbuffer is 0, 5, C5, 81.How to figure out what is wrong here, is there an ...

BPutt.1 by Associate II
  • 7797 Views
  • 10 replies
  • 0 kudos

Resolved! VL53L8CX DEEP SLEEP MODE

Hello, I'm trying to set up the deep sleep mode for VL53L8CX using NUCLEO L476RG board so as described in the datasheet that it can operates in 3 different states:• Wake-up: The device is set in HP idle (high power), waiting for instructions.• Sleep:...

ali6 by Associate II
  • 2458 Views
  • 4 replies
  • 0 kudos