Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Clarification on Time-of-Flight Cover Glass

Hi,  I was reading @John E KVAM excellent post on Time of flight sensor glass:https://community.st.com/t5/mems-and-sensors/time-of-flight-cover-glass/ta-p/49259and this documentationhttps://www.st.com/content/ccc/resource/technical/document/applicati...

J1234_0-1727837224035.png J1234_1-1727837305511.png
J1234 by Associate
  • 1293 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CX IO

 Hi Team, We are using the VL53L4CX in QCS8550 platform.Below are queries listed below for clarification. Query 1:Load Capacitance I'm using a same I2C for 5 sensors of VL53L4CX. Is that good to connect or any load capacitance issues will occur Need ...

VL53L8CX motion detection

Hi! I am trying to use motion detection data from VL53L8CX sensor. Where can I find deeper explanation of results data and configuration structure than is it in datasheets.RESULTSstruct{uint32_t global_indicator_1;uint32_t global_indicator_2;uint8_t ...

MSkrt by Associate II
  • 1837 Views
  • 1 replies
  • 0 kudos

Resolved! VD56G3 MANUAL_COARSE_EXPOSURE Register Clarification

I have the STEVAL-56G3MAI1 evaluation kit for the VD56G3 image sensor and the STEVAL-EVK-U0I1 to connect and take snapshots from the sensor.  I have been looking into script generation and register setting and I would like to set the exposure time to...

astral256 by Associate II
  • 1280 Views
  • 2 replies
  • 1 kudos

Resolved! Measuring Multiple vl53l4cd on single i2c line

I am currently implementing a series of  vl53l4cd sensors into a project. These work really well and I am able to address these individually on one shared i2c line. These sensors are working perfectly fine on this shared line when measured independen...

VL53L8CX no i2C connection

I have a VL53L8CX time of flight sensor connected via I2C on a custom board. The Board has other devices that can talk on I2C no problem. now i cant see the i2c address of the ToF device. from my understanding everything seems to be fine and in accor...

AA.16 by Associate III
  • 3749 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L7CX on STM32H7 with en.STSW-IMG037

Hi:I am trying to use en.STSW-IMG037 (VL53L7CX_GUI_v2.2.29009) software to evaluate the VL53L7CX ToF sensor. I implemented firmware on the NUCLEO-H755ZI-Q board with VL53L7CX sensor from Pololu based on the firmware example in the "en.X-CUBE-TOF1\Pro...

pshih_0-1725888373318.png pshih_1-1725888589020.png
pshih by Associate II
  • 4166 Views
  • 6 replies
  • 0 kudos

Resolved! Cannot read more than one zone with VL53L3CX

Hello,We have been using multiple VL53L3CX sensors for some time but only using one zone. Now, we want to use all four of them but we are running into some issues: Specifically, we can only read one zone while the rest all return status 255. In addit...