Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

10x10 Multizone Ranging on VL53L1 GUI not working

Hi,I have an X-NUCLEO-53L1A2 and a NODE_F401RE.The VL53L1.exe GUI is unstable and frequently freezes, but I could at least perform most of my experimental measurements (including MultiZone Ranging 4x4).However, when using MultiZone 10x10 Ranging, the...

kunf_0-1731692667339.png
kunf by Associate
  • 1375 Views
  • 2 replies
  • 0 kudos

Resolved! Vl53L1X Calibration Issues

We have two VL53L1X sensors side by side. Both have gilizmo cover glass and are placed 140mm from a 8.5x11 sheet of mat grey paper. Running the calibrate offset function returns 2mm for sensor one and 6mm for sensor two. Following this the Xtalk cali...

Resolved! Multizone sensor calibration buffer

Dear forum,I try to understand the bin shape of the VL53L8CX / CH sensor calibration buffer while evaluating different sensor cover and their influence on ranging. Using the example8 file from the ULD driver the shape looks more or less always the sa...

_jh by Associate II
  • 2601 Views
  • 5 replies
  • 1 kudos

Resolved! TOF VL53L5CXV0DH/1 bad detections with status 255

I’m using a VL53L5CXV0DH/1 sensor in my current setup (see pictures). The goal is to detect a ball rolling between the sensor and the background. The red box is about 12cm apart.The settings is 4x4 for speed, i also noticed that 60 is not the highest...

thumbnail_IMG_7547.jpg IMG_7543.jpg 2024_11_15_15_42_31_workspace_1.5.0_NIC_TOF_rev001_Core_Src_tof.c_STM32CubeIDE.png 2024_11_15_15_22_40_workspace_1.5.0_NIC_TOF_rev001_Core_Src_tof.c_STM32CubeIDE.png
sde c.1 by Senior II
  • 2005 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L4CX: How/where to store calibration data

I need to calibrate a VL53L4CX and have been reading UM2923. The functions described do not seem to bear any obvious relationship to the functions in the STM32Cube middleware which was generated for my project, which I find confusing. I it is not cle...

VL53L3 Linear Detection of Target

Hi everyone,I know there are 25 and 35 degree detection angles of VL53L3. I am aware that this situation is a mechanical situation. But I want to make a timing gate and find people's speeds. We have submitted our product to reliability and validity t...

fafeyto_0-1730290638557.png
fafeyto by Associate II
  • 1402 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1 calibration using water target surface

Hello again!I've been trying to measure water level using the VL53L1 sensor and reading forum posts on it, and I've gathered that RefSPAD calibration isn't really recommended anymore.From my research on the topic, I know that water reflects only 2% o...

LDMigotto by Associate II
  • 2160 Views
  • 1 replies
  • 1 kudos