Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L8CX ToF Sensor

Hi. I have question regarding VL53L8CX ToF sensor. The minimum distance is 2cm. The space between the objects being measured is less then that. Was wondering if it will be possible to reflect the light off from a mirror at 45 degrees to increase the ...

vl53L4CD GUI Not starting/opening

Hi,    i do not seem to be able to use the application gui for the vl53L4CD Nucleo board.    when i try and open the application i get this message. is anyone familiar with this issue?     

Afam_Nwokolo_0-1739982556393.png

Resolved! X-NUCLEO-53L8A1 with NUCLEO-F401RE on Ubuntu

 Hello everyone,I am very new to the STM ecosystem and don’t know much about it. I am using an Ubuntu PC and trying to work with the X-NUCLEO-53L8A1 expansion board and NUCLEO-F401RE.There is a software package available for VL53L8CX to detect the pr...

kgb by Associate III
  • 1626 Views
  • 2 replies
  • 2 kudos

Connect SATEL board? MZ-AI EVK

I want to connect a vl53l8 satel board to the x nucleo 53L8A1, and I want to use the MZ-AI EVK software to record measurements of the external sensor, is this possible?

ay0and0 by Associate II
  • 898 Views
  • 1 replies
  • 0 kudos

Sensor to detect plastic film, edge detection

Hello,  Could someone please recommend a TOF sensor(or other) for reliable plastic sheet detection.Application: Measure the width of a sheet or film of plastic in production environment.  We would use  two sensors to detect the edges of the film.  We...

MyMack by Associate II
  • 4597 Views
  • 12 replies
  • 0 kudos

About VL53L4CX -Getting the best single-target data

Hi,I have two questions to ask.1、How do I adjust "VL53LX_MAX_RANGE_RESULTS"and "VL53LX_MAX_USER_ZONES" if I want to get a best single target of data?Would it be better to change them all to 1? It's not in the manual.2、VL53L1CB has a single-target get...

Wwei by Associate
  • 1762 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L0X - measuring ball position in plexiglass tube

We are trying to assemble a laboratory plant from https://github.com/gergelytakacs/AutomationShield/wiki/FloatShieldThe ball position sensor (VL53L0X) is positioned at the top of the transparent policarbonate tube. We checked the reported ball positi...

71251627-26342300-2323-11ea-9496-1c5d9f2872e3 results_sensor.png
matevzb by Associate II
  • 976 Views
  • 1 replies
  • 0 kudos