Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to troubleshoot I2C bus sensor response problem?

I have a project where I am attempting to use six ST Microelectronics VL53L0X Time-of-Flight (ToF) sensors grouped into two 3-element arrays for position/orientation sensing on an autonomous wall-following robot. I originally had both arrays installe...

FPayn.1 by Associate III
  • 3601 Views
  • 5 replies
  • 0 kudos

Sensor test with evaluation cards

I am currently in the process of doing a study on the VL53L0X, VL53L1X, VL6180X, VL6180 sensor I carry out distance and air gap tests on each sensor, the goal is to choose the ideal sensor to carry out proximity detection for the access control. So I...

MSAMB.1 by Associate III
  • 1160 Views
  • 1 replies
  • 0 kudos

Vl53L1X Velocity Measurement

Apologies if this is a dumb question or fairly simple. I plan to use the VL53L1X to measure the velocity of an object for a university project and was wondering if there is a way to extract the velocity of the object from the distance/range measureme...

GEl-S.1 by Associate
  • 2025 Views
  • 3 replies
  • 0 kudos

vl53l0x stopped working suddenly !

vl53l0x was working good at start. I have connected i2c thermal camera in parallel with vl53lox sensor.. It was working good for past 3days.and then suddenly sometimes it stops updating the reading. When i restart it, it was working normal. Suddenly ...

Yadav by Associate II
  • 3091 Views
  • 4 replies
  • 0 kudos

Multiple vl53l1x sensor

Hello , I need to use 2~3 vl53l1x sensor breakout(from pololu) with nodemcu32s ,use arduino ide , My code is below, It work fine if I only use one chip ,​#include <Wire.h> #include <vl53l1_api.h>   VL53L1_Dev_t dev; VL53L1_DEV Dev = &dev;   int statu...

0690X00000ArJNKQA3.jpg