Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.
Hello,I am building an IoT level sensor for a vessel. The vessel is emptied at the bottom, and I would like to sense how much stuff is still in there from the top lid. The tank is approximately 40cm deep, and 10x10cm wide and it is dark inside.Consid...
I want to implement LIDAR using multiple VL53L3CX.I have two questions about VL53L3CX.first,In the previous case of VL53L1X, LIDAR was implemented by setting an ROI.As far as I know, VL53L3CX does not have the function to set ROI.Indeed, is there no ...
Hi,I have a project with VL6180X sensor. Moving from first prototype to second revision, I have realized that I have no use for AWS sensor. Therefore I can switch the sensor to the non-AWS having, also cheaper VL6180V. Datasheets of these sensors are...
vl53l0x interfacing STM32F7I used Pololu libraries and replaced read and write functions with HAL functions, at first it worked properly for several hours, but after that it stopped working and returned 8191 value, after two hours it started working ...
I see from this GY530 schematic that the module has level converters for the I2C lines, but not for GPIO & XSHUT lines. When using a 5V micro-controller like an Arduino UNO or MEGA to run multiple VL53L0Xs using XSHUT to configure addresses, will dr...
What is the difference betwen Long DM and Short DM in terms of principle of operation?For example in ULD API for Short Distance Mode these registers are used:status = VL53L1_WrByte(dev, PHASECAL_CONFIG__TIMEOUT_MACROP, 0x14); status = VL53L1_WrByte(d...
I can use this senser only together ST micro controller.Also its freeware APIs not enough for this purpose.I think ST must provide neccessary support about this subject without need anycustomer feed back.( Because VL53L1X is belong you )Regards.
I have a single 'known good' VL53L0X hooked up to an Arduino Mega 2560 through a bidirectional level shifter. When I attempt to initialize it I get the following output:Opening port Port open Arduino Hex VL53L0X Demo In Adafruit_VL53L0X::begin(29,1,...
Hello I am new in the field of Tof sensors I would like to know how you proceed to carry out your calibrations? are there any software manipulations to perform? I read in a conversation in which you spoke about function and variable Xtalk .. If so, p...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.