2018-12-17 7:43 AM
Hi all
Have a look @
https://www.st.com/resource/en/application_presentation/teseo-3-quick-testing-guide.pdf
it's an easy way to test the connection to the Teseo III server based Assisted GNSS without special equipment and/or tool.
2019-03-12 8:02 AM
I am trying to use this guide to test access to the server and am having trouble. We are using the Teseo-LIV3F device. I have been able to get a password from the device using the $PSTMSTAGPS8PASSGEN command. But trying to access the server using that password and device id returns a 401 Unauthorized.
Application note AN5160 sections 4.1.1.4 implies that a password needs to be assigned by a location.io administrator. Is this no longer true and there is no requirement to first contact location.io?
2019-03-12 8:10 AM
Hi
The AN5160 is a generic application note which covers all the TeseoIII IC and modules.
In case of TeseoIII IC a dedicated account has to be provided for each customer.
In case of Teseo-LIV3F, the module has a dedicated account assigned on location.io system.
You can follow the presentation (link) to test your access to location.io.
Thanks
Regards
Francesco
2019-03-12 8:18 AM
Hello,
Okay so that is good to know. So this is what I am attempting to test from a PC running Ubuntu. I'm using Curl but without the proxy setting. Can you look at this and tell me if I'm doing something incorrectly?
curl --verbose --header "Content-Type: application/json" --header "Accept: application/json" --header "Authorization: RXN-SP cId=ZYDLLXxEH94dEeX2,mId=MYST,dId=00513730383638361400759E,pw=xrhjr7hbCP464UpZdA0Oxearolh8DX++JpbRXdwxcJk=" --data "[{\"ee\":{\"version\":8,\"constellations\":[\"gps\"],\"seedAge\":0}}]" http://stm.api.location.io:80/rxn-api/locationApi
* Trying 72.51.26.210...
* TCP_NODELAY set
* Connected to stm.api.location.io (72.51.26.210) port 80 (#0)
> POST /rxn-api/locationApi HTTP/1.1
> Host: stm.api.location.io
> User-Agent: curl/7.58.0
> Content-Type: application/json
> Accept: application/json
> Authorization: RXN-SP cId=ZYDLLXxEH94dEeX2,mId=MYST,dId=00513730383638361400759E,pw=xrhjr7hbCP464UpZdA0Oxearolh8DX++JpbRXdwxcJk=
> Content-Length: 59
>
* upload completely sent off: 59 out of 59 bytes
< HTTP/1.1 401 Unauthorized
< Content-Language:
< Content-Type: text/html
< Date: Tue, 12 Mar 2019 15:14:22 GMT
< Content-Length: 994
<
* Connection #0 to host stm.api.location.io left intact
<!DOCTYPE html PUBLIC "-//W3C//DTD XHTML 1.0 Strict//EN" "http://www.w3.org/TR/xhtml1/DTD/xhtml1-strict.dtd"><html xmlns="http://www.w3.org/1999/xhtml"><head><title>Error report</title><style type="text/css"><!--H1 {font-family:Tahoma,Arial,sans-serif;color:white;background-color:#525D76;font-size:22px;} H2 {font-family:Tahoma,Arial,sans-serif;color:white;background-color:#525D76;font-size:16px;} H3 {font-family:Tahoma,Arial,sans-serif;color:white;background-color:#525D76;font-size:14px;} BODY {font-family:Tahoma,Arial,sans-serif;color:black;background-color:white;} B {font-family:Tahoma,Arial,sans-serif;color:white;background-color:#525D76;} P {font-family:Tahoma,Arial,sans-serif;background:white;color:black;font-size:12px;}A {color : black;}HR {color : #525D76;}--></style> </head><body><h1>HTTP Status 401 - Unauthorized</h1><hr/><p><b>type</b> Status report</p><p><b>message</b>Unauthorized</p><p><b>description</b>This request requires HTTP authentication.</p><hr/></body></html>
2019-03-12 8:27 AM
Looking the field they seem correct to me.
Did you evaluate the <gpsTime> to create the password? It's the current time expressed in the number of seconds since midnight 06-Jan-1980
Thanks
Regards
Francesco
2019-03-12 8:42 AM
That leads me to a question. Do I need to update the password every time I access the server? If so, how many seconds is a password valid for? Right now for my test I'm doing things by hand. Sending the command to the chip on our board, then copy/paste the result into my PC to run the command.
I tried the test again with keeping the time as close as possible and it still failed. I'm using the GPS seconds reported from this web site http://leapsecond.com/java/gpsclock.htm
I did experiment with the $PSTMSTAGPS8PASSGEN and it returns the same password for wide ranges of seconds but does eventually change with a large enough number change. So I'm guessing that the same password is valid for some length of time.
2019-03-12 8:53 AM
Okay, so that website was giving me a bad number for seconds. :) I found the right value and generated a password and it worked fine.
But I still have the question of how long a password is valid for? I'll probably reset it everytime we power up so not a big issue.
Thanks for your help.
2019-03-12 12:57 PM
Okay, so I have a response coming back from the server now. But I'm a little confused about what to do with the data coming back. I see some NMEA commands listed to program seeds. I see the command $PSTMSTAGPSSEEDBEGIN, $PSTMSTAGPSBLKTYPE can be used. I assume this is programmed with the "seed" value coming back in a JSON response?
Does this data require an initial general location? (i.e. using cell site or wifi address)
There is also a command $PSTMEPHEM, which can program ephemeris data? Is this command still used?
2019-03-13 1:11 AM
Hi
> Do I need to update the password every time I access the server?
Yes. You do.
> If so, how many seconds is a password valid for?
each password is valid several minutes (~10 minutes)
Regards
Francesco
2019-03-13 1:25 AM
Ciao
From location.io you can access two kind of data:
Which data you download depends on the HTTP_REQ you did.
iolocation provides you a JSON file.
The JSON file has to be parsed to fill the '$PSTMSTAGPSSEEDBEGIN, $PSTMSTAGPSBLKTYPE' (for Extended Ephemeris) or $PSTMEPHEM (for Real Time data) command and inject the data into the Teseo-LIV3F.
BUT the JSON-File description is under NDA (you can read a subset in the AN5160 which is public)
To avoid NDA as ST we prepared a prebuilded library available in the X-CUBE-GNSS1 (the STM32 drivers but the Library is ARM-Cortex-M0 oriented to be portable) to provide a library which parses the JSON file and injects the data in Teseo-LIV3F
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.