2025-01-07 4:48 PM
Hi I'm now using Teseo-VIC3DA through evb.
I have a curiosity about which level the sensor fusion btw GNSS and IMU is performed.
I can log the data through Teseo suite application.
But i can't figure out that GNSS messages such as NMEA GNGGA, GPVTG etc... is the result of fusion or the raw data of GNSS.
Those messages is the result of fusion btw GNSS and IMU?
And if that data is the result of fusion, Is there any other way to get raw GNSS data?
Thanks a lot in advance.
Solved! Go to Solution.
2025-01-15 9:25 AM
In VIC3DA, GGA messages are sensor fusion messages.
If you need pure GNSS message, you can look at PSTMDRGPS message being output. This will output GNSS only fixes.
For this you need to enable CDB-ID 228 [bit 23]
$PSTMSETPAR,1228,0x800000,1
$PSTMSAVEPAR
$PSTMSRR //save and reset for setting to take effect
// After device is reset
$PSTMGETPAR,1228 //read back to make sure bit is set
Just so that you are familiar with setting CDB registers and reading register settings back, please refer to "Section 10.2 STM system configuration commands"
2025-01-15 9:25 AM
In VIC3DA, GGA messages are sensor fusion messages.
If you need pure GNSS message, you can look at PSTMDRGPS message being output. This will output GNSS only fixes.
For this you need to enable CDB-ID 228 [bit 23]
$PSTMSETPAR,1228,0x800000,1
$PSTMSAVEPAR
$PSTMSRR //save and reset for setting to take effect
// After device is reset
$PSTMGETPAR,1228 //read back to make sure bit is set
Just so that you are familiar with setting CDB registers and reading register settings back, please refer to "Section 10.2 STM system configuration commands"
2025-01-15 4:34 PM
Thx a lot for reply.
I have some more questions.
Is there any other reason that raw message's ID include "DR" which means Dead Reckoning?
And I try to activate some messages like $PSTMPVRAW.
I activate that message with command $PSTMSETVAR and confirm that parameter is changed with command $PSTMGETPAR.
But the problem is that i can't view the message with the Terminal in Teseo-Suite.
Are the messages that can be activated with command predetermined?
2025-01-17 9:43 PM
Hi,
Could you please let me know what command you sent to enable $PSTMPVRAW?
Let me try on VIC3DA and I will let you know.
2025-01-18 11:42 PM
Hi,
I use command
$PSTMSETPAR,1228,6cce6000
to configure
Thank you
2025-01-22 8:14 PM
Hi,
Can you please make sure you are using the latest software version?
This is the version I am running (refer to BINIMG version)
$$PSTMVER,GNSSLIB_8.4.19.27.11_ARM*66
$$PSTMVER,GNSSLIB_8.4.19.27.11_ARM*66
$$PSTMVER,OS20LIB_4.4.0_ARM*40
$$PSTMVER,GPSAPP_2.14.0.11_VIC3DA_ARM*30
$$PSTMVER,BINIMG_4.6.18.11_VIC3DA_ARM*3F
$$PSTMVER,SWCFG_8406532d*34
$$PSTMVER,STAGPSLIB_6.0.1_ARM*5B
$$PSTMVER,DRLIB_2.14.1_ARM*7E
$$PSTMVER,STA8090_922bc043*60
If not, can you please upgrade the software using Teseo Suite to the one on the website? https://www.st.com/en/embedded-software/teseo-vic3dsw.html
Once you do that if you set CDB bits accordingly, you should see PSTMPVRAW being output.
Is there any other reason that raw message's ID include "DR" which means Dead Reckoning?
No special reason except it pertains to Dead Reckoning.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.