2019-06-11 4:31 AM
Hi,
Doing randoms tests on the TESEO III accuracy, I've found an horizontal accuracy of 14m for 95% of the locations with extremes of 23m. Does ST have more informations about the TESEO III accuracy ? Are there tests that have been published ?
Thanks
Regards
2019-06-11 5:09 AM
I'm sure they have published CEP specs.
Your results do seem particularly awful, but I think that's on you and your antenna or RF side. Does not seem consistent with a properly executed test. When people generate spec numbers it is usually with very expensive and very well placed antennas to provide optimal results.
I've posted plots to this GNSS subforum.
2019-06-11 5:25 AM
https://community.st.com/s/feed/0D50X00009ZEutBSAT
CEP99 well inside 5m, and the bulk of the hits well inside 2.5m
Make sure you don't have airflow over the IC or TCXO
2019-06-11 6:08 AM
Thanks !
Are you using SBAS ?
2019-06-13 5:51 AM
Ciao
Teseo3 in the default configuration guarantees:
and we are close to
I think there something strange in your platform.
SBAS is On by default in ST firmware.
Regards
Francesco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.