2023-12-19 12:47 AM
Hello,
How can I check that the teseo correctly receives L5 band satellite and not only L1?
Is it indicated in a NMEA message?
Best regards
Mich
2023-12-19 4:01 AM
Newer form of GSV should have additional field at end indicating constellation and band.
2023-12-19 7:01 AM
From UM3009:
SignalID Decimal, 1 digits An identifier to indicate the signal in use. Currently it is 1 for GPS, GLONASS, 2 for
BEIDOU and QZSS 6 for GALILEO
What do you want me to do with that?
$GPGSV,1,1,04,24,78,311,40,23,33,265,23,10,25,307,29,14,08,047,23*74
2023-12-19 8:53 AM
>>What do you want me to do with that?
I don't know, you asked the question about what NMEA Sentence you'd find this information in.
The default is for NMEA-0183 v3.1, you will need to switch to V4.10 to get the Signal ID. That will also change the PRN/SV numbering schemes.
TESEO III used the following for NMEA V4.10
$PSTMSETPAR,1122,4
$PSTMSAVEPAR
$PSTMSRR
NMEA-0183 V4.10 and V4.11 have different designations for other bands, GPS L5I is 7, GPS L5Q is 8, for example.
I'm not sure NMEA is entirely fit for purpose 4 decades onwards, perhaps there are some binary messages you can decompose for signal usage at a constellation / band level?
2023-12-19 11:50 PM
Thanks a lot Tesla,
Can I use the same $PSTMSETPAR,1122,4 command for teseo-liv4f?
This command is not listed in the UM3009 document.....
Is this command for NMEA-0183 V4.10 or V4.11?
Best regards
Mich
2023-12-20 12:40 AM
The $PSTMRF message contains a frequency field (software manual, pdf page 42). You can enable the $PSTMRF field with the 0x80 bit mask on CDB-ID 201. I don't have an L5 antenna right now so I don't know if it will list a satellite twice if it's receiving its L5 frequency. I'll be happy to post a test sample in about a week using an L1&L5 antenna that's in the mail.
2023-12-20 1:34 AM
However I am currently unable to get the $PSTMRF message through a $PSTMNMEAREQUEST or through CDB201. In fact, I cannot get any $PSTM messages to come out of the Teseo-LIV4F.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.