2019-07-02 8:14 PM
I dont have have one of the boards the documentation said.. however i have a ftdi which i am connecting to CN9 arduino ports i have it connected to D2 of the GNSS to my RX pin of the ftdi and D8 of the GNSS to the TX of my FTDI device.
I dont see any data been transmitted once i power it up.. am doing it wrong?
2019-07-02 11:43 PM
Hi
Sorry I'm not understanding which board are you using?
Is it the X-Nucleo-GNSS1A1?
BTW in any case to get the module working you have to guaratee:
which these condition the module is up-and-running and it will transming NMEA message on the UART (pins tx-2_rx-3 @9600)
Regards
Francesco
2019-07-03 7:14 AM
That worked... Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.