2019-11-24 5:15 AM
2019-11-25 12:31 AM
Hi Dror
> Can TeseoV support RTK internally?
TeseoV will support RTK internally through third partners.
For further info please contact ST Local team.
Thanks
Ciao
Francesco
2019-11-24 6:35 AM
I don't believe so. There are firmwares to allow for raw measurements, which you'd then have to push into RTKLIB, or something similar, or post process.
I didn't have any joy getting the firmware, and other industry contacts suggested the data was quite noisy when compared to competitive solutions. The Broadcom device was also not great.
The Teseo V might be a better implementation to pursue. You need to be a customer of some merit to get access. ST isn't very supportive of the maker community in the GNSS/RTK space.
Using uBlox ZED devices here, in single and dual antenna configurations, the F9K is an automotive part with an IMU and wheel-tick/direction input, the F9R is a more consumer device basically integrating RTK and untethered dead-reckoning with an internal IMU
2019-11-24 7:51 AM
I would like to see an official and a definitive answer from ST guys in this forum.
Thank you.
2019-11-25 12:10 AM
Hi Dror
As official answer I can say:
therefore if you are looking for a ready-to-be used RTK-solution... I'm sorry TeseoIII is not enough.
While if you are designing a platform with an external MCU which could run an RTK algorithm (i.e.: http://www.rtklib.com/) in this case TeseoIII can provide to the MCU the raw measurement data the RTK-algorithm needs.
Hope this helps
Regards
Francesco
2019-11-25 12:16 AM
Ciao Francesco,
Can TeseoV support RTK internally?
Thank you,
Dror.
2019-11-25 12:31 AM
Hi Dror
> Can TeseoV support RTK internally?
TeseoV will support RTK internally through third partners.
For further info please contact ST Local team.
Thanks
Ciao
Francesco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.