| Subject | Author | Posted | |
|---|---|---|---|
|
I am getting an error when working through the README.HOW_TO.txt in linux-stm32mp-6.1.82-stm32mp-r2...
| 2024-10-22 8:19 PM | ||
|
I have started working on STM32MP257f board. I have installed open st linux distribution package on...
| 2024-10-20 11:56 PM | ||
|
Hello, I am using meta-st-stm32mp which points to mickledore and is using linux 6.1.82. I woul...
| 2024-10-07 1:56 AM | ||
|
How can I enable the HDMI output log at boot? I want to see the login promt at the HDMI output.
| 2024-10-02 3:30 PM | ||
|
I want to display the loop log at start up from UART to the HDMI. How can i achieve that? Is it so...
| 2024-09-29 2:09 PM | ||
|
Hello everyone, we have developed a custom board based on stm32mp157 chip. We have also forked the...
| 2024-09-18 8:25 AM | ||
|
i am planning to build an dpoae device so which one do u prefer STM32MP157D-DK1 processor or STM32H...
| 2024-09-18 12:08 AM | ||
|
Has anyone encountered issues with unstable clock configuration on the STM32MP135F? I'm having trou...
| 2024-09-17 4:24 AM | ||
|
Hello everyone,
I am trying to program the STM32MP157 to control a simple LED using Keil software...
| 2024-09-15 5:30 AM | ||
|
Hi, I am debugging the STM32MP257F-EV1 board with a debugger via JTAG/SWD. The kernel version is 6...
| 2024-09-14 11:22 AM | ||
|
Many examples use UART4 as debug output, in my particular design, UART4 are in an inconvenient loca...
| 2024-09-05 5:39 AM | ||
|
Hi, i am facing the issue with the header file like I am using ADC pin where i facing the issue wi...
| 2024-09-03 5:11 AM | ||
|
Hi! I having a question. I'm using STM32MP151 processor and my initrd won't work because it got st...
| 2024-09-01 4:57 PM | ||
|
NOTICE: CPU: STM32MP157FAC Rev.Z NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board...
| 2024-08-20 12:14 AM | ||
|
Hello to everyone! We have develop a System on Module board based on the STM32MP153AAB. Currently ...
| 2024-08-15 1:59 PM | ||
|
I want to test the memory by using U-boot. I'm reading the DDR memory from 0xC0000000 to 0xE000000...
| 2024-08-15 3:34 AM | ||
|
Hello, Would it be possible to have an updated guide on how to use a custom device tree within my ...
| 2024-07-29 7:26 AM | ||
|
Hello, Would it be possible to have an updated guide on how to use a custom device tree within my ...
| 2024-07-29 7:04 AM | ||
|
Hello, Would it be possible to have an updated guide on how to use a custom device tree within my ...
| 2024-07-29 6:57 AM | ||
|
Hello STM Community, I am considering using the STM32MP157F-DK2 as a platform for a LoRa gatewa...
| 2024-07-25 10:27 PM |