| Subject | Author | Posted | |
|---|---|---|---|
|
hellow I have a project about kinematic of a drone.Is good solution the :https://www.st.com/en/eva...
| 2024-12-29 3:19 PM | ||
|
I follow the instruction in this git repository to build an openWRT image for STM32MP157F-DK2. I us...
| 2024-12-25 1:30 AM | ||
|
Using OSTL 4.1.2 and build DISTRO=openstlinux-weston MACHINE=stm32mp15-disco on STM32MP157F-DK2. Fo...
| 2024-12-24 11:52 PM | ||
|
I am doing with stm32mp157f-dk2 i got succeed with understanding a bit about openstlinux stuffs ...
| 2024-12-12 9:03 PM | ||
|
Hi, I have a STM32MP157F-DK2 and I can't install anything on the card, especially python3-pi...
| 2024-12-12 8:00 AM | ||
|
Hello We have a few questions regarding LPDDR4 memory configurations, and we would appreciate your...
| 2024-12-03 9:14 PM | ||
|
Hi All, I have custom phycore stm32mp13 based carrier board and i want to create uboot splash scre...
| 2024-12-01 10:56 AM | ||
|
Hello, I run make for install USB wifi driver for STM32MP1. I had import enviroment, but i can't m...
| 2024-11-27 1:31 AM | ||
|
Hi All, I am working on enabling and testing the LCD (RGB666) and backlight (enable and pwm) funct...
| 2024-11-24 2:03 PM | ||
|
Hi there, I am working on a product where we use the STM32MP157C for our purposes At the moment w...
| 2024-11-22 4:33 AM | ||
|
Hi, We are wondering that do we support to boot uboot from nand flash then boot into OS from exter...
| 2024-11-21 7:39 PM | ||
|
Hello: I am debugging the network development of STM32MP135 bare metal, using the protocol stack...
| 2024-11-21 9:04 AM | ||
|
We are using STM32MP!57A processor in our custom board. In this we are unable to read t...
| 2024-11-20 5:52 AM | ||
|
Hello, I have a STM32MP2 platform with A/B partitioning for TF-A, metadata and FIP. I'm looking f...
| 2024-11-18 6:30 AM | ||
|
Hello! If I run the openAMP example I can see the two new devices appear in the linux /dev folder:...
| 2024-11-12 5:08 AM | ||
|
Hello, We are evaluating the X-STM32MP-GNSS1 eval board on STM32MP-157F-DK2. The X-STM32MP-GNS...
| 2024-11-12 3:33 AM | ||
|
I'm working with the STM32MP131FAE in a bare-metal environment, and I'm experiencing issues ...
| 2024-11-11 2:19 AM | ||
|
Hello, I am developing on the STM32MP131FAE board in a bare-metal environment. This chip does not...
| 2024-10-30 10:20 PM | ||
|
Description: I'm working with the MYIR MYD-YA157C board, based on the STM32MP157C, and experiencing...
| 2024-10-26 3:07 AM | ||
|
I am trying to connect to audio codecs to give 4 channel of audio on a MP257. Can I connect SAI2.SC...
| 2024-10-23 7:52 AM |