2025-08-27 1:32 PM - edited 2025-08-27 3:14 PM
Clicking on a user's name to view their profile, I can see their previous posts. For example:
It says the last reply to the thread was a week ago. However, when viewing that thread, there are 4 more replies after mine. The latest reply should reflect the last such reply.
How widespread is this problem? 2/4 of the posts from this user show a "latest reply" which is not the latest.
I viewed a few other user profiles and could find the same problem happening. Probably 25% or so are wrong. Here are a few:
2025-08-28 4:34 AM
Hi @TDK,
Thanks for bringing this up!
To replicate this:
Questions:
I’ve raised this topic with our vendor to see if there are any issues with this component.
I will get back once I have news.
Regards,
Lina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.