2025-02-21 9:55 AM - edited 2025-02-21 9:56 AM
If an ST member accepts a solution on a thread to which I've replied, the "latest notification" box on the main forum page shows as if it was my answer that got accepted:
when in fact it wasn't:
On the notification screen, it correctly shows that a solution was accepted.
I'm aware that this can happen if a user accepts one solution and then changes it, in which case only the last one shows as accepted. However, if my solution is accepted, I get an email, and I did not get one in this case. It also happens a fair amount.
This may only happen when an ST employee accepts a solution.
2025-02-21 10:34 AM - edited 2025-02-22 5:38 AM
Hello @TDK
I can confirm this behavior on my side, and I think my college @Lina_DABASINSKAITE will take care of it.
PS: for the answer I’ve marked, I don’t think it is the best. It was just a wrong click that I’ve removed.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-25 5:20 AM
2025-02-25 5:29 AM
Seen this also on occasion. Assumed a number of best solutions had been selected at different times, with only last sticking
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.