2023-07-28 6:44 AM - edited 2023-07-28 6:46 AM
I've clicked on the "bell icon" *after* I've seen this "new notification" on the frontpage.
I've even force-reloaded the notification feed page, but it did not change.
No big loss, just another example that Khoros is just another overjavascripted crap.
JW
2023-07-28 7:28 AM
... and yes, it *did* appear in the list later, but I did not check, when.
JW
2023-08-06 11:37 PM
Thanks for reporting this. Could you please confirm if it was only one-time thing or you see it constantly with all notifications? I've tried to test on my side but usually the notifications are displayed correctly in the feed.
Michael
2023-08-07 11:18 PM - edited 2023-08-07 11:20 PM
Hi Michael,
No, I don't make a deliberate observation like this regularly, nor do I intend to watch actively for occurence of this.
This is obviously consequence of unnecessarily complicated design which ultimately will lead to the same modes of failure than jive and salesforce did. It was your choice, without listening to users, again.
JW
2023-08-13 12:39 PM
Please let us know if you notice a similar issue with any other notification and we'll try to investigate further. Unfortunately for now we are not able to reproduce this issue.
Michael
2023-10-26 3:30 AM
Hi @waclawek.jan ,
Thank you for your patience and sharing your feedback. Can you tell us what browser and system you use most often when you notice such cases? This will allow us to better target our internal testing.
Best,
Adam
2023-10-26 3:52 AM
Hi Adam,
Most often?
I've noticed this once. It would be silly to expect me to check for such irregularity regularly, wouldn't it.
I usually use FF on Windows, it might've been Win8.0 or some flavour of Win10.
JW
2025-09-09 2:05 AM
OK so I've just noticed the same thing happening.
JW
2025-09-09 2:39 AM
It did appear eventually in the list, but later than I made that post above (I *did* reload that list *after* I made the post at 11:05, just to be sure).
I've noticed it only when the next item arrived into it, at 11:39, did not look at it meantime.
JW
2025-09-09 3:15 AM - edited 2025-09-09 3:18 AM
Not sure if this is quite the same:
On the left (the main forum front page), it says it's a "Reply"; on the right (the notifications feed), there is a "Moved" notification - but no "Reply"
PS:
If I look in the thread, there is no reply from @Maxime_MARCHETTO
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.