2022-02-20 8:10 AM
Hello, everyone.
I had a problem with version 7.1.0 of X-CUBE-AI.
When I load the TFlite model of the neural network and generate the code I have problems initializing the input and output buffers. In particular I have a problem with this assignment: ai_buffer ai_input[AI_NETWORK_IN_NUM] = AI_NETWORK_IN;
The compiler gives me a problem with the AI_NETWORK_IN macro, which is listed as deprecated and returns ai_buffer*. Has anyone else encountered the same problem? How can it be solved?
In version 5.20.0, I had no problems with initialisation and already evaluated many different examples.
Thank you,
Davide
Solved! Go to Solution.
2022-03-04 7:40 AM
Hello Raggio,
I don't know when you use this assignment, but now since 7.x, the macro "AI_NETWORK_IN" is mapped on a function (ai_network_inputs_get()). Now to create the handle of the IO tensor before to use them with the ai_network_run() fct, the following typical code is expected:
/* Array of pointer to manage the model's input/output tensors */
static ai_buffer *ai_input;
static ai_buffer *ai_output;
vois aiInit() {
...
/* Reteive pointers to the model's input/output tensors */
ai_input = ai_network_inputs_get(network);
ai_ouput = ai_network_outputs_get(network);
...
}
/*
* Run inference
*/
int aiRun(const void *in_data, void *out_data) {
/* 1 - Update IO handlers with the @ of the data payload */
ai_input[0].data = AI_HANDLE_PTR(in_data);
ai_output[0].data = AI_HANDLE_PTR(out_data);
/* 2 - Perform the inference */
n_batch = ai_network_run(network, &ai_input[0], &ai_output[0]);
if (n_batch != 1) {
err = ai_network_get_error(network);
...
};
...
return 0;
}br,
Jean-Michel
2022-03-04 7:40 AM
Hello Raggio,
I don't know when you use this assignment, but now since 7.x, the macro "AI_NETWORK_IN" is mapped on a function (ai_network_inputs_get()). Now to create the handle of the IO tensor before to use them with the ai_network_run() fct, the following typical code is expected:
/* Array of pointer to manage the model's input/output tensors */
static ai_buffer *ai_input;
static ai_buffer *ai_output;
vois aiInit() {
...
/* Reteive pointers to the model's input/output tensors */
ai_input = ai_network_inputs_get(network);
ai_ouput = ai_network_outputs_get(network);
...
}
/*
* Run inference
*/
int aiRun(const void *in_data, void *out_data) {
/* 1 - Update IO handlers with the @ of the data payload */
ai_input[0].data = AI_HANDLE_PTR(in_data);
ai_output[0].data = AI_HANDLE_PTR(out_data);
/* 2 - Perform the inference */
n_batch = ai_network_run(network, &ai_input[0], &ai_output[0]);
if (n_batch != 1) {
err = ai_network_get_error(network);
...
};
...
return 0;
}br,
Jean-Michel
2022-03-10 8:11 AM
Thank you Jean-Michel,
Your solution is right, thank you for the answer.
Best Regards,
Raggio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.