2021-10-14 1:25 PM
I'm trying to validate on target the example proposed in https://www.youtube.com/watch?v=k8AAr84z27s concerning the asc NN implementation with X-CUBE AI.
My target is the NUCLEO-F401RE instead.
After generating code I try to build and I get the warnings:
..........................................................................................
../Core/Src/main.c:179:13: warning: 'MX_GPIO_Init' defined but not used [-Wunused-function]
179 | static void MX_GPIO_Init(void)
| ^~~~~~~~~~~~
../Core/Src/main.c:146:13: warning: 'MX_USART2_UART_Init' defined but not used [-Wunused-function]
146 | static void MX_USART2_UART_Init(void)
| ^~~~~~~~~~~~~~~~~~~
../Core/Src/main.c:120:13: warning: 'MX_CRC_Init' defined but not used [-Wunused-function]
120 | static void MX_CRC_Init(void)
............
c:\st\stm32cubeide_1.6.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: ./Core/Startup/startup_stm32f401retx.o: in function `LoopFillZerobss':
C:/Users/marco/STM32CubeIDE/workspace_1.6.1/testing ai sound/Debug/../Core/Startup/startup_stm32f401retx.s:100: undefined reference to `main'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:66: testing ai sound.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
...........................................................................................................................
Launching the program I get: Program file does not exist
C:\Users\marco\STM32CubeIDE\workspace_1.6.1\testing ai sound\Debug\testing ai sound.elf not found
I updated to PE64 Windows binary parser, but without success.
What can I do? Thanks
2021-10-14 2:43 PM
>>Why .elf file does not exist ?
Because the linker didn't get closure and so didn't generate it?
It's complaining it can't find a main() function.
Do you have one in your compiled files? Are you using C++ / .cpp files?
2021-10-15 3:16 AM
Thanks DeLorean.
The reason was the Application Structure of STM32CubeMX.
It was selected the option "Do not generate the main ()"
Now I get this warning instead:
"c:\st\stm32cubeide_1.6.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: ./X-CUBE-AI/App/app_x-cube-ai.o: in function `MX_X_CUBE_AI_Init':
C:/Users/marco/STM32CubeIDE/workspace_1.6.1/test ai ASC/Debug/../X-CUBE-AI/App/app_x-cube-ai.c:73: undefined reference to `MX_USART2_UART_Init'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:66: test ai ASC.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
12:02:28 Build Failed. 3 errors, 0 warnings. (took 2s.464ms)"
and USART2 is the standard COM port for NUCLEO-F401RE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.