2020-07-07 8:30 PM
[webinar - Program decision trees in sensors with a Machine Learning Core]
2020-07-07 8:32 PM
MLC can work at four different data rates: 12.5, 26, 52, 104 Hz. Data logs should be provided at one of these rates during the MLC configuration procedure.
Besides these limitations, the sensor itself can work even at higher data rates, after the MLC has been configured, since the MLC will process data at its own rate.
Together with MLC, also additional features (like filters, FIFO, FSM, etc..) can be configured on the sensor. When both FSM and MLC are enabled, a merge tool has to be used in Unico to generate a configuration including both features.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.