cancel
Showing results for 
Search instead for 
Did you mean: 

Unicleo-GUI not Detecting my NUCLEO-IKS01A3 Board

ZoeTakacs
Associate II

Hi all, 

I installed Unicleo-GUI on my Windows laptop, and was able to read sensor data from my NUCLEO-IKS01A3 board successfully. The board was automatically identified by the software as being connected to COM4 yesterday. For some reason today the software recognizes the COM connection but not the board and thus won't display the data being read by it on the screen. 

I have tried reinstalling Unicleo as well as the FP-SNS-DATALOG2 function pack with no success. 

Any advice or suggestions are appreciated!!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

The firmware from FS-SNS-DATALOG2 is not compatible with Unicleo-GUI. Compatible firmware is in X-CUBE-MEMS1 package.

View solution in original post

2 REPLIES 2
Miroslav BATEK
ST Employee

The firmware from FS-SNS-DATALOG2 is not compatible with Unicleo-GUI. Compatible firmware is in X-CUBE-MEMS1 package.

Federica Bossi
ST Employee

Hi @ZoeTakacs ,

Did you try to use the compatible firmware that Miroslav suggested you?

If yes, remember to click the 'accept as solution' button on his answer to be of help to other users :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.