2023-12-26 12:29 PM - last edited on 2023-12-28 9:17 AM by STTwo-32
Hi,
I have generated n-classification library file from NanoEdgeAI. for NUCLEO-L476RG Development board. I have included the knowledge.h and NanoEdgeAI.h files in Inc folder as shown in the tutorials. I have added libneai.a file to Src folder. I am getting "undefined reference to `neai_classification_init'" error.
Please help.
Soumadeep De
Solved! Go to Solution.
2023-12-28 9:07 AM
Hello @SoumadeepDe ,
Did you add the library to path in the project settings? if not you can refer to this thread which explain the method to add the Lib.
BR
2023-12-28 9:07 AM
Hello @SoumadeepDe ,
Did you add the library to path in the project settings? if not you can refer to this thread which explain the method to add the Lib.
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.