2020-07-12 5:40 AM
Hello,
I am currently working with the acoustic scene classification (ASC) of the FP-AI-SENSING1 project.
I tried to load the tflite model, which is provided at: STM32CubeFunctionPack_SENSING1_V4.0.2\Utilities\AI_Ressources\models\asc_keras_mod_93_int8.tflite
Unfortunately, I always end up with this error: ValueError: quantized_dimension must be in range [0, 1). Was 3.
I always end up with this error no matter which tensorflow version I use.
Can anybody help me with this issue?
Thanks in advance,
Ilkay
2020-07-13 1:05 AM
Hello Ilkay
The FP pack at the time used the following requirement tensorflow==1.14.0
I tried to load the tflite model in this way:
Python 3.7.3 (default, Mar 27 2019, 22:11:17)
[GCC 7.3.0] :: Anaconda, Inc. on linux
Type "help", "copyright", "credits" or "license" for more information.
>>> import tensorflow as tf
>>> interpreter = tf.lite.Interpreter(model_path="asc_keras_mod_93_int8.tflite")
INFO: Initialized TensorFlow Lite runtime.
>>> interpreter.allocate_tensors()
>>> input_details = interpreter.get_input_details()
>>> output_details = interpreter.get_output_details()
>>> print (input_details)
[{'name': 'conv2d_11_input', 'index': 3, 'shape': array([ 1, 30, 32, 1], dtype=int32), 'dtype': <class 'numpy.int8'>, 'quantization': (0.050990983843803406, 42)}]
>>> print (output_details)
[{'name': 'dense_12/Softmax', 'index': 12, 'shape': array([1, 3], dtype=int32), 'dtype': <class 'numpy.int8'>, 'quantization': (0.00390625, -128)}]
>>>In this way I have no issue , you may want to use the same set up than I .
good luck
L.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.