2026-05-11 7:10 AM - edited 2026-05-11 8:32 AM
Hello,
I am trying to create a project with Cube AI studio v1.2.
My toolchain and libraries are well detected with Cube AI studio v1.1, and I can create a project.
However, it is not the case for the Cube AI studio v1.2. The toolchain paths seem valid, but when creating a project no IDE is proposed at all, as shown in the attached image.
Could you help me please ? No debug logs are generated.
Versions :
Solved! Go to Solution.
2026-05-11 8:42 AM
Thank you for your response.
Updating proxy settings on each involved application has actually solved my problem.
I guess it couldn't download any updates, hence this bug. It has also solved the unwritten log files bug.
I have added the versions of each tools in the initial post, just if needed for the other users.
Thank you very much for your help !
2026-05-11 7:37 AM
Hello @stm-trt ,
Could you share what are the dependencies version you have for
- STM32CubeIDE
- STM32CubeMX
You also mentioning that you don't have any logs. Does it mean that the folder C:\Users\<username>\.stm32cubeaistudio\logs is empty ?
If yes, could you check that all instances of STM32Cube AI Studio are killed in the Task Manager and the folder .stm32cubeaistudio is writable ?
Best regards,
Yanis
2026-05-11 8:42 AM
Thank you for your response.
Updating proxy settings on each involved application has actually solved my problem.
I guess it couldn't download any updates, hence this bug. It has also solved the unwritten log files bug.
I have added the versions of each tools in the initial post, just if needed for the other users.
Thank you very much for your help !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.